Tool/software:
The customer want to use part of the channels as high side switch or low side switch.
Whether we have some guidance for the hardware circuit design and the software diagnostics description like(Open Load Detection)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The customer want to use part of the channels as high side switch or low side switch.
Whether we have some guidance for the hardware circuit design and the software diagnostics description like(Open Load Detection)?
Hey Fabio,
Sure, that is fine. They can use each 1/2 bridge independently for whichever load.
For hardware design see this:
Best Practices for Board Layout of Motor Drivers (Rev. B)
System Design Considerations for High-Power Motor Driver Applications
And here's a file for offline open load and short circuit detection:
0675.DRV87xx-Q1_Offline_OL_SC.pdf
Best,
Jacob