Part Number: DRV2700
Other Parts Discussed in Thread: TINA-TI
Tool/software:

We are attempting to drive a haptic actuator. VD is at 5 volts. The amplifier seems to be attenuating the signal rather than amplifying, on top of that there is a notch at around 200 hz. I am drawing my signal from laptop Aux out. Cin was chosen based on the input impedance of the Amp to give a filter roll off at 15hz. The boost section seems to be working fine, voltage accross CBoost a good 103 as intended. From the internal schematic of the IC I cannot understand what's going wrong if the boost section is fine. We also tried with Ren as 10k to set enable only after powering the chip, that did not change much.
I wonder if there's any trouble with the batch of ICs we have, we tried it out with 3 different boards, the one of them was overheating under no input, the other two were exhibiting notching and attenuation. Could any process during manufacturing the PCBs have damaged the IC?