Hi,
DRV8412 datasheet says the output rise and fall time is typically 14 ns. i measured on the eval board with a motor load. The rise and fall time is pretty close to the specification. my question is that with so fast rise and fall time for motor drive applications will EMC/EMI be a concern? if yes, do you have any experience with any EMI supression component? let's a L-C-L type EMI supression filter is used, do I still need the power ferrite bead for overcurrent protection? as the EMI supression filter will slow down the output current rising rate as well.
Thanks
Best regards
Gordon