Tool/software:
As dispicted in DRV8251AEVM user guide, Pot1 controls the PWM signal that goes into IN1, by turning it clockwise you increase the duty cycle from 0% to 100%. But when I use this evaluation board to drive a motor or coil, I can't get a PWM output, which duty cycle is from 10% to 100%, from OUT1 test point. The PWM duty cycle is only from 0% to 47% when I turn the Pot1 Potentiometer clockwise. How can I get a 100% duty cycle PWM output?
In the period of test, the Pot2 is always 0% (no turning) and Pot3 is turn to 100% clockwise. The supply voltage is 24V.