Other Parts Discussed in Thread: DRV8434S,
Tool/software:
Hello
I am evaluating your DRV8434S solution, and have made software to control it.
I have tested that all the signals are ok, and the SPI communications are also verified. However there is no output generated on the motor side.
I used a logic analyzer to check and verify the Enable, nSleep are both High. The STEP signal is 50% duty cycle, 1kHz.
All the VREF, VSDO are measured 3.3V.
I just wonder even if I don't configure the chip through SPI, I should still be able to generate some output on the motor, right? Since we have pulses on STEP.
We have tried different microstep, current settings, none of them actually worked.
So what could be the root cause?
Thanks in advance!
Best regards
Weinan