Tool/software:
Hello,
I use a DRV110 for driving a solenoid, with a peak current of 5A and a hold current of 2A. The currents measured are correct, but I have an issue with the keep time. When the part is cold, at room temperature, the keep time is much lower than expected, and the time increases after one or two minutes of use and stabilizes. I have noticed that the keep current is much larger when the part is cold.
Is this a known issue ? I changed several times the DRV110 itself and more or less all parts without success.
Thank you for your help because I am stuck with this issue.
Schematic diagram:
Results of measurements: