This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8432 for stepper motor

Other Parts Discussed in Thread: DRV8412, CONTROLSUITE

Hi,

I'm trying to to drive a stepper motor with 30V and 2A (5A peak). I have chosen Mode M1=M2=M3=0. But I don't  know which singanls I have to input to PWM_X pins 

 Is it possible to have some timing diagrams for the input and output in my case ?

Thank you,

Yury

 

  • Yury,

     

    I suggest you take a look at the DRV8412-C2-Kit.  The DRV8412 might be able to handle the job based on the ratings you list above and is the "little brother" to the DRV8432. 

    All the example code, documentation, GUI, etc. are available for free as a reference on ControlSUITE.  You will see a link to ControlSUITE and the DRV8412-C2-Kit at the link below:

    http://www.ti.com/tool/drv8412-c2-kit