This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316C-Q1: Maximum RPM of motor -- over 30000RPM not possible with TI BLDC?

Part Number: MCF8316C-Q1
Other Parts Discussed in Thread: MCF8316A

Tool/software:

Hi TI, 

Along with the MCF8316A, I'm trying to understand whether or not the BLDC driver will be suitable for our needs. The specs for the brushless direct current motor with Hall Sensors are included below. The vendor of the identified motor have stated that in their experience, 30000rpm is the limit with TI BLDC drivers. The motor max is 60000rpm. Are you able to point me to any data that shows this should work, or point me to an alternative integrated BLDC that would work? Please let me know what additional info you may need. 

Number of pole pairs: 1

Phase to Phase Resistance: 0.238ohms

Phase to Phase Inductance: 0.0202mH

Maximum speed: 60000rpm

Nominal Supply Voltage: 24VDC

Thanks!