This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8243-Q1: DC Motor Driver Integrated Device Proposal Request

Part Number: DRV8243-Q1
Other Parts Discussed in Thread: DRV8245-Q1

Tool/software:

Hi,

The customer will consider developing an electric side step for the car.

Please recommend a product that meets your requirements.

1. Operating voltage range: 9 to 16V

2. Limit voltage: 40V (LOAD DUMP PASS will be possible)

3. Applied motor rated specification: DC motor, 12V / 5.5A

4. Stall current: 12A or higher

5. Operating temperature: -40 to 90 degrees

6. Current monitoring (suggestions to distinguish between monitored and non-monitored products)

7. Motor driver drive power ON/OFF function (feature supported product, non-supported product suggestion)

8. Package integrated type will be reviewed first (motor driver + drive FET integrated)