This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983: DRV10983: DRV10983 repeatly spin for a while then stop

Part Number: DRV10983

Tool/software:

Hi

I asked a question in this link before, but unfortunately I did not get my answer. I had a experience with DRV10983 and Nanotec motor.

When I set the following values in registers, the motor spins continuously (it doesn't stop after a few seconds). so the problem mentioned in the link, doesn't appear. However the speed is not controlled. This problem occurs only in closed loop and not in open loop ... if I change register for closed loop, the motor doesn't spin correctly and that problem appear again. What should I do?

#define REG_20  0x1D
#define REG_21  0x2E
#define REG_22  0x49
#define REG_23  0x00
#define REG_24  0xC0
#define REG_25  0xFF
#define REG_26  0x88
#define REG_27  0xF4
#define REG_28  0xAE
#define REG_29  0xC9
#define REG_2A  0x0C
#define REG_2B  0x0D

Thanks

regards,

Diba