Part Number: UC2625-EP
Tool/software:
Hello,
We are using UC2625MDWREP as a commutation chip which generates gate pulses for High side and low side outputs for controlling three phase BLDC Motor. With UC2625MDWREP , max 20V motor can be directly connected , but we have a requirement of 400V.
Motor requirement is as follows:
Voltage - 400V
Current - 5A
Is there any gate driver IC along with integrated mosfets which takes the gate pulses from UC2625MDWREP to control the motor.