Tool/software:
Hello,
I am trying to make my own bldc motor controller, and I am using the DRV8329AEVM for its power MOSFETs and gate drivers. For the MCU, I am using the F28035 Piccolo card (not the launch pad that connects easily with the DRV8329AEVM pins). I am trying to connect the pwm signals from the f28035 to the INHx and INLx pins of the EVM. Whenever a voltage is applied to the INHx and INLx pins, the nfault is toggled and the gate driver appears to be disabled (all the GHx pins read 6 volts and all the GLx pins read 0 volts). My question is what might be causing this? Can I use the f28035 microcontroller or is the EVM only compatible with the LAUNCHXLF280049C LaunchPad?
Thank you in advance for any Help!