Tool/software:
Hi,
Q1
We have confirmed that there are plans to release a jig like a Gang programmer for mass production programming in Q2 2022. Any updates on this? We are looking for a mass production programming tool for the MCF8316A.
Q2
When using the built-in BuckRegulator, if it is not used externally and is only used to supply to the internal DVDD, how much current capacity should we estimate?
When using the built-in BuckRegulator, if it is not used externally and is only used to supply to the internal DVDD and AVDD, how much current capacity should we estimate?
Q3
When using the built-in BuckRegulator, is it correct to understand that the output to AVDD is 20mA MAX external plus the internal DVDD consumption current = 170mA Ext/Load output?
Also, if used under the conditions surrounded by the red frame in the table below, the external L is 600mA (MAX?), so would it be okay to use something rated at about 1A? Are there any recommended coil conditions?
Q4.
In the case of the circuit below, the internal DVDD is supplied from the Buck Regulator, but how much current does the DVDD consume (Typ, MAX)?
Thanks,
Conor