Tool/software:
HI
My drivers is configured to 35Khz, slew rate 200V/usec.
with PWM setting of 95% the output current is not reaching the Ilim value, and I see output of ~50% of the Ilim.
is it possible that the drivers Delay compensation prevent me to reaching High DC (Duty cycle).
i.e - if the driver is set to 35Khz, and delay compensation is 1.2usec--> it's about 10% of the 28uSec cycle time.
in previous setting of 0 delay compensation and 25V/usec - I didn't have such a problem.