Other Parts Discussed in Thread: LAUNCHXL-F280049C, DRV8328,
Tool/software:
Hi
I am new to BLDC motors i am using LaunchXL-F280049C and DRV8328AEVM and trying to control a 3 phase 2 pole motor. i am able to connect the GUI and the board properly but when i turn on the power supply it gives me an error. The DRV8328 fault turns on and the following error shows up in the bottom of the GUI.
Would appreciate any help to resolve this issue. It is the same if i connect or don't connect the motor.
Thanks in advance.