Part Number: DRV8718-Q1
Tool/software:
hi expert
i want to use 1pcs 8718 to drive 5 motors. requirement is shown below:
1. Motor1 and motor2 need forward and reverse turn, but motor1 and motor 2 are not used at the same time.
2. Motor3 and motor4 need forward and reverse turn, but motor3 and motor 4 are not used at the same time.
3.Motor 5 need forward and reverse turn
4.one of M1 and M2, one of M3 and M4, M5 are all used in some time.
i have the following solution. is it suitable?