Other Parts Discussed in Thread: SFRA, LAUNCHXL-F280039C, LAUNCHXL-F280049C, DRV8323, LAUNCHXL-F28P65X, C2000WARE
Tool/software:
Hi TI experts,
We are working on the Dual-Axis Motor Drive Using Fast Current Loop (FCL) and SFRA on a Single MCU Reference Design example. this example was built on LAUNCHXL-F280049C but we want to run it on LAUNCHXL-F280039C so we edited linker cmd file. previously we used BOOST-XL-3PHGANINV driver board, and we were able to do things well.
now we want to change the driver to BOOST-XL-DRV8323RH and so we changed the Pin mappings and pin configurations accordingly based on schematics.
When we are trying to Run the motor, the motor is drawing high current and going into fault condition. Hardware is working fine. we have cross checked the hardware using The Universal Motor Control Lab example.
What are the other changes that are needed to be done. If we want to change the GAIN/IDRIVE/VDS how are they to be addressed?
thanks & regards
Raghu