Tool/software:
Hi,
The design condition was 160,000pps, but due to the constraints of the evaluation board, it was confirmed at 65,536pps or less. The pulses/second is assumed to be 160,000pps, but the maximum ƒSTEP is stated as 100kHz in 6.3 Recommended Operating Conditions of the DRV8452/62 data sheet.
Q1. Is 160,000pps pulses/second an operation that exceeds the recommended operation? Should it be kept within the 100kHz recommended in the data sheet?
Q2. Data sheet 6.3 states "STEP input can operate up to 500 kHz, but system bandwidth is limited by the motor load". What does this mean?
Q3. If there is anything I should check to prevent loss of synchronism, I would appreciate your advice.
Q4. From what I can see from the data sheet, it seems that when using the silent step function, loss of synchronism detection cannot be used. Is it possible to use the silent step function and loss of synchronism detection at the same time? I would like to control the motor to suppress the driving noise while avoiding step-out.
Q5. From what I can see from the data sheet, it seems that the overcurrent threshold cannot be adjusted. Can the overcurrent threshold be set by the user?
Finally, I would like to send you the motor test environment (which includes internal company information), so could you please approve my private message?
Thanks,
Conor