This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8452: DRV84XX-DRV89X2-DRV82X2-EVM-SOFTWARE Tuning Guide

Guru 12135 points
Part Number: DRV8452
Other Parts Discussed in Thread: DRV8462EVM, DRV8462

Tool/software:

Hi,

Could you provide a tuning guide for DRV8452 or a development guide using the GUI (DRV84XX-DRV89X2-DRV82X2-EVM-SOFTWARE)? I would like to clarify what steps are required for the development flow.

Thanks,

Conor

  • Hi Conor,

    All information necessary to develop an application with the DRV8452 is provided in its datasheet. In addition to this, a DRV8462EVM is available for product evaluation. The DRV8462EVM uses a DRV8462 DDW package, a superset stepper driver device which is 100% functional compatible with the DRV8452 in DDW package. The DRV8452 is also available as subset options. The DRV8462EVM user's guide available on the EVM webpage, describes how to use the EVM with the DRV84xx_DRV82x2_DRV89x2-EVM-GUI, https://www.ti.com/tool/DRV8462EVM. The EVM user's guide can be viewed and downloaded from, https://www.ti.com/lit/pdf/slou558

    In addition to this the EVM webpage has the EVM hardware design files and EVM firmware source code for download. For users interested in the auto-torque feature of this device this application note will be of additional help, https://www.ti.com/lit/an/slvaff1/slvaff1.pdf. Thank you.

    Regards, Murugavel