Tool/software:
What is the unite for the initial learning current? mA or what?
The same question is for ATQ_TRQ_MIN, Auto Torque Count Lower Limit.
What is the unit?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Fabio,
The values marked in yellow in the below snippet are current scaling factors for the set motor current based on VREF voltage. Current IFS (A) = VREF (V) / KV (V/A). These values are 8-bits wide, 0 will correspond to 1/256 x 100% of the set current and 0xFF or 255 will correspond to 256/256 x 100% of the set current. For the initial learning current this scaling factor is calculated as = ATQ_LRN_MIN_CURRENT (register value) * 8.
Auto torque initial learn current scaling factor (ATQ_LRN_MIN_CURRENT (register value) * 8) must be > ATQ_TRQ_MIN scaling factor and (Auto torque initial learn current scaling factor + Current steps to learn) must be < ATQ_TRQ_MAX scaling factor.
Regards, Murugavel