Part Number: DRV10983EVM
Other Parts Discussed in Thread: DRV10983, USB2ANY
Tool/software:
Hi,
I have installed the DRV10983 GUI using the program "Setup_DRV109xx_EVM.exe". After installing the GUI, I installed LabView using "LVRTE2014_f2Patchstd.exe". After restarting Windows, I launch the GUI with "DRV109xx EVM". It states "Default Config File Created", then I select Device "DRV10983" and click "OK". Then the program completely hangs with a spinning blue circle. The Window below is all I see. To fix this, I uninstalled LabView, uninstalled DRV109xx_EVM, restarted Windows, then re-installed DRV109xx_EVM, then re-installed LabView 2014. Again, the DRV109xx GUI just hangs on the image below. When I click on the image below, Windows reports "DRV109xx EVM is not responding. Close the program".
How do I fix this problem?
Thanks.
-Peter