This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983: Evaluation Module GUI File

Part Number: DRV10983

Tool/software:

Hello E2E Experts,

Good day.

I am looking for the TelcoMotion DT4260.csv because the DRV10983 EVM GUI software asks for it as described in "User's Guide - SLOU393C–July 2014–Revised January 2014" Pag 15:

" Switch back to the Basic Settings tab. Load the parameters for the supplied motor. Select Load, and a
new window appears. Depending on which motor the kit came with, select the associated file. See
Figure 9 and Figure 10 for the different motors and their accompanying file names. Both files are
located in the downloaded GUI software folder. Browse to the folder and select the correct file name
for the motor. Click Okay to configure the registers for the motor provided."

Regards,

TI-CSC