Other Parts Discussed in Thread: MCF8315C, MCF8315A
Tool/software:
Dear Reader,
We have developed a design using the MCF8316A, but during the software development process, we came across the following forum posts:
These posts are somewhat outdated, but they suggest that the errata issues have been addressed.
Question 1: Are the errata issues mentioned in these posts resolved in the current release of the MCF8316A? (This post kind of makes it look like it is: MCF8316A Fixes for Errata in Production Version)
We have purchased a couple of EVM boards to test and tune our motor.
The motor runs smoothly most of the time, but occasionally it locks up during operation, drawing all available power from the PSU (which then limits the current).
Question 2: Do you have any suggestions for resolving this issue? Could it be related to the errata mentioned earlier?
Question 3: Would the MCF8315C or MCF8316A be a suitable choice for driving this motor?
Our original plan was to use the MCF8315C instead of the larger MCF8316A.
Question 4: Are there any disadvantages to using a larger driver than necessary (apart from cost)? We typically run our motor between 3W-10W @14V.
Question 5: If the errata are still present in the MCF8316A, have they been addressed in the MCF8315C?
Question 6: Is the limited availability of the MCF8315C due to it being a new product, or are there other supply chain issues affecting stock?
Question 7: Is there an EVM board available for the MCF8315C? I could only find one for the MCF8315A.
Thank you for your assistance and advice.
Best regards,
Koen