Part Number: DRV8434AEVM
Other Parts Discussed in Thread: DRV8434EVM, , DRV8434A
Tool/software:
I installed DRV8434EVM software driver and enabled immediate execution at the end of the installation.
In this case, the DRV84XX EVM software worked as expected.
Then I closed this software window and tried to run the same software from the icon ("DRV84xx 0.1.4") that the installation created.on my desktop,
In this case, the software didn't run - didn't open the same window as previously was opened successfully.
I also tried to run it as administrator or from the location of the launcher.exe file but it didn't help.
I am trying to find what can be the reason that the same software that run successfully at the end of the installation failed to run from the "DRV84xx 0.1.4" shortcut.
Thanks in advance,
Rami