Tool/software:
Hi team,
I see we recommend to use DRV8412 to support TEC control. can you help to see if we have better choice here to meet below application request?
A TEC driver chip is required, and the specific selection requirements are as follows
1. Support 3.3V power supply voltage;
2. Support differential ±2.1 V TEC drive voltage output;
3. Output current capability > 1.1A (application scenario: at 25°C, the TEC internal resistance is 1.229Ω~1.502Ω);
4. It is best to support NTC detection function.