Tool/software:
Hello!
I have a DRV8262VEVM that was recommended to me for my load. The load varies quite a bit, from 3A to around 20A...
I have setup everything to communicate with the EVM and have the EVM connected to a small motor, everything working great! I can control the speed, ramp, brake, and everything....
But it cannot handle my 3A motor... I have the motor on a small gearbox freewheeling and directly from the power supply, the motor draws 3A max...
When I try to enable it with the EVM, it jerks slightly then just stops. The current on the GUI monitor shows 2.6A, but the motor doesn't spin...
There is no fault or error message of any kind...
Is there a physical current limit somewhere that would be set at 3A?
I thought this EVM is supposed to be capable of like 32A in parallel mode with the big heatsink...