*********** Interested in working with a TI FAE to possibly visit site and view DRV8811EVM Board in action and test results ***********
I have two questions for the DRV8811:
1.) Decay Setting - The setting for the decay signal on the DRV8811 is not clear. The setting can be slow, mixed, and fast. These setting affect the RMS current on AOUT1 and control the chopping waveform riding on each step as the signal approaches to 0V. The datasheet does not specify how to choose the decay voltage setting against a motor. Or how to select a setting that best fits a motor. What would be the best setting? Are there any actual waveforms of how AOUT1 should look with the selected settings? How much chopping should be apparent on the steps (other products do not show as much chopping).
2. ) Thermal Characteristics - In testing the DRV8811, the component heat up when the part is enables and no steps are set to the device. Can you explain why the part heats up when there are not step signals set to the device. When steps are applied the part cools down. (Interesting picture below of DRV8811EVM with removed DRV8811)
The DRV8811EVM board settings were as follows : Motor attached NEMA23, PS AMP=.33A, VREF(V)=1.33V, Motor AMP=1.6635A, Decay (V)=2.46V, DECAY=SLOW, STEP SIZE=HALF (USMO=0V,USM1=3.3V), DIR=0V, STEP=0V, Enablen=0V, Resetn=3.3V, SRn=0V, Sleepn=3.3V, Date=10/18/2011 .