Part Number: DRV8701EVM
Other Parts Discussed in Thread: DRV8701, CSD18532Q5B
Tool/software:
Hi,
From the DRV8701EVM, the continuous current is 15A and peak current 20A.

Looking at the schematic of DRV8701EVM, the Vref is left floating, thus the current chop is calculated to be 0A?
Then for the Vdsocp for DRV8701 is fixed to be 1V, and mosfet used in the EV kit is CSD18532Q5B with 2.5mohm Rdson, the OCP is calculated to be 400A.
Can you please advise what am I missing in this case and how do you achieve the claimed 15A continuous and peak current 20A as described in the features?
Best Regards,
Amirul