Other Parts Discussed in Thread: DRV8834
Tool/software:
Hi,
Customers have encountered some questions while testing the DRV8834, please help them.
1.During the motor rotation, there will be an overshoot and undershoot on Aoutx or Boutx pins, their peak voltage is depend on the current periods. The waveforms in next slide are tested with Vbus = 3.3 volts.The overshoot is up to 4 volts and undershoot is down to -0.7V.
Note: “Tip and Barrel” approach is already used to measure SW voltage waveform.
Question 1: Why there is such a phenomenon, whether it will cause IC anomalies and how it should be eliminated.
2.In DRV8834 datasheet, M0 and M1 Pins have nominal pull-downs internally, when M0 pin is floating and MO pin voltage is measured at 1.4 volts instead of being internally pulled low.
Question 2: Is this abnormal?