This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I did not see any information about IHOLD timing. Only see IHOLD_SEL = 1 or 0
Does it mean the IHOLD time = tDEAD – tDRIVE_N ?
Above is the scope shot I get, Am I understanding correctly that the period of time of Tdrive and IHOLD ?
Above setting is Idrive = 125mA and Tdrive = 321ns without pre-discharge settings and IHOLD = 0
Hi Tim,
There is no specific timing values given as this TDRIVE architecture timing is based on user control, but the sequence is the same regardless.
Does it mean the IHOLD time = tDEAD – tDRIVE_N ?
This method should provide an estimation but may not be the most reliable, as the internal timing may lag the waveforms or vary a small amount. IHOLD should not activate while the slewing is still occurring, if my understanding is correct, so you should be able to roughly determine the length given the deadtime.
May I ask the reason you are trying to calculate these specific TDRIVE states? If there is any observed issue please reach out further and I will be glad to provide additional assistance.
Best Regards,
-Joshua