This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8304: BLDC motor Driver

Part Number: DRV8304
Other Parts Discussed in Thread: DRV8328, DRV8323

Tool/software:

Hi 

Could you help to suggest suitable products

The requirements of FPV drone ESC are as follows:

Input voltage: 2S ~ 6S (7.4V ~ 25.2V) Continuous current: 55A Burst current: 65A Support current meter: 200 scales

Type: 4 in 1 (that is, integrating 4 sets of BLDC motor ESC on one board at the same time)

Control: 6 step control TI official website DRV8304 contains a gate driver (external MOSFET) that can only drive a 3-phase BLDC motor

https://www.ti.com/product/DRV8304#product-details

Does TI have a motor driver IC that can drive more than 2 BLDCs?

This application is to drive 4 BLDCs. Does TI have a 4-in-1?