Tool/software:
Hello,
set Burst as below. Why is the output value of Delay different from the setting value of Duration?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
set Burst as below. Why is the output value of Delay different from the setting value of Duration?
Hello,
This is due to the sample frequency. These 100 ms parameters are default GUI values set from a 300300 Hz sample frequency, but the sample frequency is actually set to 500000 Hz. 500000 Hz will have a duration and delay of ~60 ms. If you change the sample frequency, change it back to 500000 Hz, and select a different burst (so the GUI updates its high level page) you will see the duration and delay set to roughly 60 ms.
Regards,
Sydney Northcutt