This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV3245AQ1: DRV3245 6PWM controlling ASIL level

Part Number: BOOSTXL-DRV3245AQ1

Tool/software:

Hello

For DRV3245, can the function of controlling the DRV3245 output(GHA/GLA/GHB/GLB/GHC/GLC) through 6 PWM channels(INHA/INLA/INHB/INLB/INHC/INLC) fulfill ASIL D ?

  • Hello, 

    Thank you for your question! The DRV3245 is designed to target automotive safety applications with system level safety requirements up to ASIL D, including using 6x PWM mode. 

    Since the DRV3245 is covered under NDA and this is a public forum, if you could direct any further questions to your TI representative and he can work with us to answer any further questions. 

    Thanks for reaching out!

    Anthony Lodi

  • for functional safety, there are two aspect need to fulfill ISO26262, 1st is the HW random failure metric shall fulfill ASILC. 2st is to avoild systematic failures, this means the DRV3245 component shall be developed according to ISO26262 ASILC. so for systematic failure of DRV3245, which features/modules/blocks are developed according to ASILC, which features/modules/blocks are developed according to QM?

  • Hello,

    Thanks for the follow up!

    Since this is a public forum and this device is covered under NDA, I will work with your TI representative to answer this question.

    Regards,

    Anthony Lodi