This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8908-Q1: What happens when VM is lower than 4.5V?

Part Number: DRV8908-Q1

Tool/software:

Hello experts,

In the datasheet of DRV8908-Q1, abs max ratings of VM is from 4.5V-40V.

What happens when VM is under 4.5V? I can easily imagine the IC will fail when over 40V is applied, but I cannot understand what happens when below 4.5V is applied.

Thanks,

Kento