This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8143P-Q1LEVM: Driver not connected Hardware not connected

Part Number: DRV8143P-Q1LEVM

Tool/software:

Hi Team,

I'm trying to work with this evaluation board  however I couldn't manage to connect it to the GUI. The status LED is  blinking and D3,D6 and D7 are constantly on. I'm using the GUI version 1.0.2, and could install software to the board using the file function but the connection is never established even though the GUI senses the board on the correct COM port. There is also an external 5V supply connected to TP18. What could be the issue?

Thanks

Baris