This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: Direct connect V5 to SLEEPn

Part Number: DRV8711

Tool/software:

Is it acceptable to connect SLEEPn directly to the V5 supply voltage.  I do not need the sleep function and want the chip enabled all of the time.  Thanks...

  • Hello David,

    In sleep mode the V5 regulator will be disabled - see below from the datasheet. So this will be a non starter, when the device is powered up V5 will not be immediately available and likely result in device in sleep forever if you tie SLEEPn to V5. You can connect SLEEPn to logic high permanently from another supply voltage source, for example from the MCU supply that's used to drive the DRV8711. Thanks.

    Regards, Murugavel