This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8889-Q1: DRV8889

Part Number: DRV8889-Q1

Tool/software:

hi expert,

Now when we are using 8889, adding a 2.2UF capacitor to the AOUT port improves EMC-CEI. Will this have a significant impact on the driver itself?

  • Hi Xujian,

    I think you may have meant 2.2 nF not uF please confirm. It is common to use capacitors on each xOUTx pin between 2.2 nF and 10 nF to mitigate EMI with certain stepper motors. Higher value capacitors than 10 nF likely will load the output FETs while it is switching and result in over current shutdown. Thanks.

    Regards, Murugavel 

  • Thank you for your reply,
    We originally used 10nF, but now we have found that increasing the ESD capacitance from 10nF can improve the low frequency exceedance of CEI. Therefore, we need to pay attention to whether there is a possibility of increasing the capacitance value。

  • Or do you have any suggestions to reduce CEI

  • Hi Xujian,

    How much capacitance is needed? Higher value is okay as long as it does not trigger a thermal shutdown in your application. At switching frequencies used for current regulation for example 30 kHz, higher value capacitors have lower reactance, Xc = 1/(2*Π*f*C). This means higher switching losses causing more power dissipation (thermals) and leading to OTS. 

    Regards, Murugavel