This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8662: DRV8662

Part Number: DRV8662
Other Parts Discussed in Thread: DRV2901, DRV2911

Tool/software:

Can DRV8662 be used to add external tr etc to increase current consumption and driving frequency, and is there a circuit diagram available?
I would like to drive approximately 20nF piezo at current 1A, frequency 40 kHz.