This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3946-Q1: DRV3946-Q1



Tool/software:

Following setup initialisation given in data sheet.

1.reading status0 register 

2.response : correct NAD address, POR set, SPI Normal response but no warning register set

3.Writing to config A0-A6 and B0 to B4 and then given CLR FAULT command CMD1 0x8000 

4. response: correct NAD address, register address correct, 16 bit data 0x0000 upon reading CMD1 register 

5 Reading status0 

response: correct NAD and  register address, but POR bit still set 

6.Reading config register shows correctly written values in those register 

I am not getting clear if device has entered in standby mode correctly or not and why POR bit is not getting clear after CLRFault And also why was warning bit not set initially as expected?

Are we missing upon some steps to be followed?

please support