Tool/software:
Hello.
If I proceed with the procedure below normally and read STATUS1,
SPI Watchdog warning appears.
How do I solve it?
Status0~2 read by SPI is C2 08 26 C3 00 20 C5 00 0B C6 04 90
8.2.4.5.2 Broadcast Deployment
1. Write CMD2 = 84h (No deployment delay) or 86h (with deployment delay) to trigger the deployment
(CLR_FAULT, LOCK_CONFIG also asserted), followed by CMD2 = 00h. Response will include previous
command content (command confirmation).
2. Wait ~1 msec or ~3 msec (depends on the DEPLOY_ISEL settings) for deployment to complete
3. Read STATUS0, STATUS2 , MEAS0 and MEAS1
4. A normal response should indicate
a. DEPLOY_SUM = 2h
b. DEPLOY_STAT = 0h
c. Deployment start time measurement - TSTART_MEAS
d. Deployment current duration measurement – TDEPLOY_MEAS
Thank you.