This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2511Q1EVM: Trying to use an external PWM signal to drive the DRV2511Q1 without the on-board MSP430

Part Number: DRV2511Q1EVM

Tool/software:

Hello!

I'm trying to use an external PWM signal to drive the DRV2511Q1 without the on-board MSP430.

I configured the jumpers on the board according to the documentation in slou448.pdf. 

I biased the (-PWM) input according to DRV2511Q1 datasheet:

Now, what about these signals?

The documentation doesn't say anything about having to configure these or anything, but maybe the ENABLE line needs to be pulled up to 3v3?

FYI, this board works just fine when I use the USB based Haptics Control PC utility and the on-board MSP430.

What am I missing?

  • Joe, 

    Thanks for reaching out and your question has been received. We will look into this and provide the feedback as soon as possible, usually within 24 hours. 

    Thanks

    Hailong

  • Joe, 

    Yes, En pin needs to be pulled up and 3.3V is fine. Other pins in your circle are used to control the switching frequency of the class D amp. You can leave them floated and their values will be default.  Below is the screenshot of the pin functions from the DRV2511Q1 data sheet.