Tool/software:
Hi Team,
What is the maximum Ivcp? I can only find this spec here but can't use for equation calculation.

If can't provide, could you please consider below scenario?
- For LSD PWM control, Ivcp= 9.2nC*60kHz=0.55mA
- For HSD PWM control, Ivcp should be same as 0.55mA
- If HSD is always on, Ivcp should be lower than 0.55mA as no switching
The real working condition is the combination of above three scenario. could you draw a conclusion that if IVCP<15mA in this case can support 60kHz fsw?

Thanks !
Best
Josh