Tool/software:
Team,
DRV8215 datasheet mentions on page 33:
7.4.2 Low-Power Sleep Mode When the nSLEEP pin is low for tTURNOFF time, the DRV8215 enters a low-power sleep mode. In sleep mode, the outputs remain High-Z and the device draws minimal current from the supply pin (IVMQ or IVCCQ). After nSLEEP is set high for longer than the duration of tWAKE, the device becomes fully operational.
Unfortunately the datasheet does not specify tTURNOFF... Customer needs to know the min. tTURNOFF time in order to use this functionality.
Can you give this specification?
BR, Walter