Part Number: MCF8329EVM
Tool/software:
Hi,
I am trying for my life to tune the multiverse of EEPROM settings for my motor using your evm, but I have no luck at all. It seems from my perspective that this part lacks alot in forms of documentation and support and a reliable EVM. I get all kinds of errors but most of them are related to different BEMF faults.
Please try and assist me. I have the following parameters on my motor;
Coil resistance: 0.26Ohm
Coil inductance 0.115mH
number of poles: 6 poles
BEMF-constant 1.32mV
Shunt resistor value: 10mOhm
Mximum rpm: 1500rpm
I have changed the hw value of the current sense resistor to 10mOhm as per recommendation, since the supplied EVM apparently is not stable with the default 1mOhm resistor. (Why did you not update the EVM hw, i bought this last week?)
Can someone at TI please send over the correct register settings to get the motor to spin? We have prototypes waiting to be sent out to our customer but right now they all seems impossible to use. I would need the complete EEPROM settings, for all registers. I am not able to figure out from the available datasheets or information myself on how to set them all up.
And also, I want to point out that the settings is full of secondary calculation needs, which are really unnessesary. I would argue that what every engineer that uses this part needs is input setting for the parameters above and not be thrown into endless calculations forth and back.