This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8718-Q1: tdead problem

Part Number: DRV8718-Q1

Tool/software:

Hi team,

Customer tested VGS waveform for GH1/GL1. They set the VGS_LVL as 1.4V. The real waveform does not match the theoretical one.

In the figure below, Tdead_d is asserted after VGS_LVL. However, in real waveform, the Tdead_d is asserted when VGS = 7V.

They set the tdead_d as 2us so the time range is matched.

Why does VGS stay at 7V for this 2us?

Regards,

Peter