This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8300: When High-side gate and Low-side driver output MOSFET short ground

Part Number: DRV8300

Tool/software:

Hi Team,

When DRV8300 High-side gate and Low-side driver output MOSFET short ground, what protection mode will be activated?

and what would happen if there was no protection?
For example, half-wave output, or the High-side gate and Low-side driver are short-circuited and burned, or the bootstrap capacitor cannot be charged, etc.

  • Let me additional information
    Case 1 : During operation, of the 6 MOSFETs, one of the high-side gate always short to PVDD(Left side figure).

    What will happen to the circuit at this time?

    Case 2 : During operation, of the 6 MOSFETs, one of the low-side gate always short to GND(Right side figure).

    What will happen to the circuit at this time?

    If there is no protection above, please describe what will happen.
    For example, half-wave output, or the High-side gate and Low-side driver are short-circuited and burned, or the bootstrap capacitor cannot be charged let high-side mosfet abnormal action, etc.

    Please take the time to reply.

  • Hi Kevin,

    Give me about a day to look into this and then provide an update.

    Regards,

    Yara

  • Hi Kevin,

    I took a look at your concerns and it looks like DRV8300 only has two protection features:

    It is one of our more simple devices, if you are looking for something that has close to the same specifications but more features I would recommend DRV835x

    If there is no protection above, please describe what will happen.
    For example, half-wave output, or the High-side gate and Low-side driver are short-circuited and burned, or the bootstrap capacitor cannot be charged let high-side mosfet abnormal action, etc.

    I can't say for certain what would happen in the event of the shorts the you are seeing but it could potentially cause abs max violations and damage the device or the MOSFETs.

    Regards,

    Yara

  • Hi Yara : 
    thanks for your reply
    I will refer to this narrative

    Regards,

    Kyle

  • Hi Kyle,

    No problem, please feel free to let me know if you have any additional questions or post a new E2E.

    Regards,

    Yara