This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8215: Datasheet error tINRUSH description

Part Number: DRV8215

Tool/software:

Team,

looks like datasheet of DRV8215 contails mismatching information on page 22:

When voltage or speed soft-start is disabled, the tINRUSH time directly reflects the setting of the TINRUSH bits. The tINRUSH can be set to a value between 5ms (corresponding to 0000h) and 6.7s (corresponding to FFFFh), with a default value of 1s. Each increment of LSB corresponds to 102.4μs of the inrush time.

The default value of the respective MSB and LSB registers is both 0x00h, so it corresponds to 5ms according to the description above and not 1s like marked in yellow above...

Which wording is correct?

BR, Walter