Tool/software:
Hello experts,
Can nSLEEP pin be pulled to low during PWM output in DRV8908-Q1?
Any concern for this?
Thanks,
Kento
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello experts,
Can nSLEEP pin be pulled to low during PWM output in DRV8908-Q1?
Any concern for this?
Thanks,
Kento
Hi Kento,
Give us 24 hours to look into this and get back to you.
Best,
Keerthi
Hi Kento,
Typically, pulling nSLEEP low while the device is driving OUTx is not a concern. However, this is dependent on the load being driven. For example, a motor could generate enough BEMF voltage while decelerating to pump the VM voltage and potentially violate the abs max rating of the device. This can be mitigated with sufficient bulk capacitance on VM or decelerating the motor before pulling nSLEEP low.
Regards,
Joshua