Tool/software:
Hello. Could you explain how the MCF8329A handles situations where the reference voltage for current sensing is not exactly 1.5V but has a slight bias?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, The reference voltage for current sense is fixed to 1.5V in MCF8329A. Can you help us to understand the difference on this bias?
Regards,
Manu
Due to the current structure of our circuit, the ground of the shunt resistor may fluctuate from noise generated when the motor is running. This could cause issues in current sensing. Does the driver have any protection features against this noise, or is there an algorithmic solution implemented for this?
Hi,
I am told by the team that there is a dynamic offset correction internal to the device which can help you if the device has a DC bias on the shunt, but we cannot compensate for any AC coupling on the shunt voltage.
Thanks and regards,
Sachin S