Tool/software:
Hello,
I have similar issue. At 24V at VM, no load, all input are pulled up, there is about 30mA consomption and the device temperature rise 30°C above the ambiant.
What could be the reason ?
Regards,
Emil
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I have similar issue. At 24V at VM, no load, all input are pulled up, there is about 30mA consomption and the device temperature rise 30°C above the ambiant.
What could be the reason ?
Regards,
Emil
Hello Emil,
Are there any load connections to the OUT1 to 4 during this test? We tested current consumption on the EVM with 24 V VM. It was compliant with the datasheet specifications. Could you please share the schematic of your application? Thank you.
Regards, Murugavel